REGEN.POWER

Description

This parameter reads regen resistor's calculated power, which is determined as follows:

(V2 / R) * DutyCycle

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Watt

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen REGEN.POWER 0x3007 0x2 UDINT - - RO True